Technical FAQs

Ask a Question

Symmetra PX; Bypass not in Range messages

 
 
 
Issue:
Symmetra PX; Bypass not in Range
 
Product line:
Symmetra PX
 
Environment:
All models, all serial numbers
 
Cause:
Bypass not in range messages are generated whenever the AC input voltage goes outside of the acceptable bypass criteria (-10%/+12%).
 
The voltage thresholds are:

Input Voltage - Normal Operation = 166-240Vac (-20/+15%) or 96-138Vac (L-N)
BYP voltage range = 187-229Vac (-10/+10%) or 108-132Vac (L-N)
Output Frequency (sync to mains) 57 - 63 Hz for 60 Hz nominal
 
This event can also be generated if the input frequency falls outside the UPS output frequency setting.
 
You can configure the output frequency on the Power View:
60 Hz +/- 0.1 Hz
60 Hz +/- 3 Hz
60 Hz +/- 10 Hz
50Hz +/- 0.1 Hz
50Hz +/-3Hz
50Hz +/-10Hz
 
For example, if the output frequency is set to 60 Hz +/- 0.1 Hz and the frequency is 60.2 Hz you will have this alarm. If you wish to adjust the output frequency you must do so in Load Disconnect mode.
 
Resolution:
No action necessary
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
Was this helpful?
What can we do to improve the information ?