Technical FAQs

Ask a Question

SSH server running after restored configuration of InfraStruXure Central

Issue:

SSH server running after restored configuration of InfraStruXure Central

Product Line:

InfraStruxure Central

Environment:

InfraStruxure Central
StruxureWare Central
StruxureWare Data Center Expert.

Cause:

If SSH is turned on, it will be turned off after the configuration is restored as this is the default setting.

Resolution:

This issue was found in ISXC 5.1.1 and the only current resolution is to manually reconfigure SSH settings.

Was this helpful?
What can we do to improve the information ?