Technical FAQs
Technical FAQs
Netbotz 455 and Netbotz 550 are now able to support Pelco IP cameras using the Rack Access PX-HID & Pod Sharing functionality.
To setup motion detection for the Pelco cameras, please open Advanced View UI and follow the below steps:
Please note that Pelco camera motion can be detected once in a 30 second window of time and each instance of motion will continue for that 30 seconds. This is a hard coded limit from Pelco