Engineering Designer Guide
The InRow Chilled Water product design closely couples the cooling with the IT heat load. This design prevents hot air recirculation, while improving cooling predictability and allowing for a pay as...
[read more]
-
App Note
-
-
Rack Air Containment Application Guidelines and Approved Configurations -
The Rack Air Containment System (RACS) is a modular front and rear plenum for use in isolating the supply and return air between an APC Netshelter SX rack enclosure and an APC InRow™ cooling solution. The containment system is designed to create a separate environment for air distribution in order to prevent mixing of hot and cold air streams, resulting in a more predictable cooling pattern. The modular design and ability to retrofit to an existing Netshelter SX rack enables medium to high density racks to be cooled in an autonomous environment without overcooling the room mixed with lower density loads.
PDF
(rev. 2)
-
Hot Aisle Containment Application Guidelines and Approved Configurations -
The Hot Aisle Containment System (HACS) is a modular ceiling panel and door system for use in isolating the supply and return air between an APC NetShelter rack and an APC InRow® cooling solution. The containment system is designed to create a separate environment for air distribution in order to prevent mixing of hot and cold air streams, resulting in a more predictable cooling pattern. The modular design and ability to retrofit to an existing Netshelter rack enables medium to high density racks to be cooled in an autonomous environment without overcooling the room.
PDF
(rev. 1)
-
Best Practices for Designing Data Centers with the InRow RC -
The InfraStruXure® InRow RC is designed to provide cooling at the row and rack level of a data center for rack based IT equipment with front to back airflow. When designing data centers with this product, there are some best practices that should be followed to ensure the InRow RC is cooling as designed. This paper presents the best practices that should be followed when designing a data center with the InRow RC, and provides some additional guidelines to follow when some of these best practices can not be adopted as part of the data center layout.
PDF
(rev. 0)
-
InRow RP-CW and InRow RP-DX Environmental Control -
The InRow RP controls the environment with four basic functions: cool, reheat, dehumidification, and humidification and various combinations thereof. This application note describes the control process for the InRow RP. In order to provide environmental control, the InRow RP units monitor the temperature and humidity of the return air, temperature and humidity of the supply air, and three remote rack inlet temperatures.
PDF
(rev. 0)
-
Data Center Humidification Strategies -
ASHRAE recommends maintaining relative humidity in the range of 40-55% at the air inlet of critical data center IT equipment. This application note first considers various methods of quantifying the expected humidification and dehumidification loads for this design humidity range. After determining latent loading, an approach to equipment selection is offered using APC-MGE InRow products; IR-RC, IR-RP and the FM product as an example.
PDF
(rev. 0)
-
Selection procedure for RC and RP -
Describes the procedure for selecting InRow Chilled Water products for successful applications.
PDF
(rev. 0)
-
PEX-AL-PEX Application -
APC uses Cross-linked Polyethylene piping as a reliable choice for distribution of water and glycol based cooling fluids through the InfraStruXure® Cooling Distribution Unit (CDU). Its construction allows flexible installation techniques that minimize joint use and prevent vibration transmission, while providing good strength and durability for system pressures under 1.03 MPa (150 psig). This paper will explain how Polyethylene pipe is made, its construction, uses, safety ratings, and design constraints associated with the material.
PDF
(rev. 0)
-
InRow RC Cooling of HP C-Class Chassis -
High performance blade chassis such as the HP c-Class are alleged to be highly problematic regarding thermal solutions within traditional Data Center spaces. APC has developed in row cooling products, such as the InRow RC, to specifically address such challenges.
PDF
(rev. 0)
-
InRow RC Environmental Control -
The function of the InRow RC product is to cool air from the hot aisle and deliver it to the cold aisle at the temperature setpoint. The InRow RC controls the environment with a cooling function only. This document describes the control process for the InRow RC. In order to provide environmental control, the InRow RC unit monitors the temperature of the return air, temperature of the supply air, and a remote rack inlet temperature
PDF
(rev. 0)
Brochure
Design/Configuration
-
Guide Spec
-
-
InfraStruXure InRow RC Guide Specifications -
CSI formatted guide specifications for the InRow RC
PDF
(rev. 0)
-
ZIP
(rev. 0)
-
InfraStruXure InRow RP Guide Specifications -
CSI formatted guide specifications for the InRow RP
ZIP
(rev. 0)
-
Submittal Drawing
-
-
ACRP500-501 - InRow RP Chilled Water -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RP
PDF
(rev. 7)
-
ACRC100 - InRow RC Chilled Water -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RC
PDF
(rev. 6)
-
ACRC103 - InRow RC Chilled water -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RC
PDF
(rev. 4)
-
ACRC500-501 - InRow RC, 600mm, Chilled Water -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RC
PDF
(rev. 2)
-
ACAC10016 - InRow RP, 36-Inches Flexible Pipe Kit -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RP
PDF
(rev. 0)
-
ACAC10017 - InRow RP, 72-Inches Flexible Pipe Kit -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RP
PDF
(rev. 0)
-
ACAC10011- InRow RC 36-Inches Flexible Pipe Kit -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RC
PDF
(rev. 0)
-
ACAC10012 - InRow RC 72-Inches Flexible Pipe Kit -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RC
PDF
(rev. 0)
-
User Manual
-
-
InfraStruXure InRow RP Tech Data (Manual) -
General Specifications; Technical Specifications; Bid Specifications
PDF
(rev. 2)
-
InRow RC Installation (Manual) -
Installation
PDF
(rev. 1)
-
InfraStruXure InRow RP CW O&M Manual -
Operation; Maintenance
PDF
(rev. 1)
-
InfraStruXure InRow RC Operation and Troubleshooting (Manual) -
Configuration; Operation; Troubleshooting
PDF
(rev. 1)
-
InRow RC and RP Metal Hose Installation (Sheet) -
Installation; General Specifications
PDF
(rev. 1)
-
InRow Cooling Unit Unpacking Sheet -
Unpack all InRow products
PDF
(rev. 1)
-
InfraStruXure InRow RC 300 mm Bridge Trough Installation (Sheet) -
Installation
PDF
(rev. 0)
-
InfraStruXure InRow RC Bridge Shielding Trough Cover Installation (Sheet) -
Safety; Installation
PDF
(rev. 0)
-
InfraStruXure InRow RC InRow Data Cable Bridge Partition Installation (Sheet) -
Safety; Installation
PDF
(rev. 0)
-
InfraStruXure InRow RC InRow Data Cable Bridge Partition, 600-mm (Sheet) -
Installation
PDF
(rev. 0)
-
InfraStruXure InRow RC InRow RC Bridge Shielding Trough 600-mm Installation (Sheet) -
Installation
PDF
(rev. 0)
-
InfraStruXure InRow RC to NetShelter SX 48U Rack Height Adapter Installation (Sheet) -
Installation
PDF
(rev. 0)
-
InfraStruXure InRow RC to NetShelter VX Height Adapter Installation (Sheet) -
Installation
PDF
(rev. 0)
-
InfraStruXure InRow RC Seismic Guide (Manual) -
Installation; Installation
PDF
(rev. 0)
-
InRow Full Rack RC Installation -
This covers the new RP CW without reheat and humidification.
PDF
(rev. 0)
-
InRow RC Technical Data Manual -
Tech Data Manual for the InRow RC ACRC100/ACRC500 series skus
PDF
(rev. 0)
-
InRow RP/RC/RD (600mm) Online Guide -
Online User's Guide
PDF
(rev. 0)
The InRow Direct Expansion product design closely couples the cooling with the IT heat load. This design prevents hot air recirculation, while improving cooling predictability and allowing for a pay...
[read more]
-
App Note
-
-
Rack Air Containment Application Guidelines and Approved Configurations -
The Rack Air Containment System (RACS) is a modular front and rear plenum for use in isolating the supply and return air between an APC Netshelter SX rack enclosure and an APC InRow™ cooling solution. The containment system is designed to create a separate environment for air distribution in order to prevent mixing of hot and cold air streams, resulting in a more predictable cooling pattern. The modular design and ability to retrofit to an existing Netshelter SX rack enables medium to high density racks to be cooled in an autonomous environment without overcooling the room mixed with lower density loads.
PDF
(rev. 2)
-
Hot Aisle Containment Application Guidelines and Approved Configurations -
The Hot Aisle Containment System (HACS) is a modular ceiling panel and door system for use in isolating the supply and return air between an APC NetShelter rack and an APC InRow® cooling solution. The containment system is designed to create a separate environment for air distribution in order to prevent mixing of hot and cold air streams, resulting in a more predictable cooling pattern. The modular design and ability to retrofit to an existing Netshelter rack enables medium to high density racks to be cooled in an autonomous environment without overcooling the room.
PDF
(rev. 1)
-
UPS Power for the InfraStruXure InRow SC -
The InfraStruXure® InRow™ SC (ACSC100 and ACSC101) is a self-contained air conditioner for server rooms and wiring closets. This application note outlines considerations for powering the unit from a UPS.
PDF
(rev. 0)
-
Guidelines for Using Rack Air Containment System with InfraStruXure InRow SC -
The InfraStruXure® InRow™ SC (ACSC100 and ACSC101) is a self-contained air conditioner for server rooms and wiring closets. This application note provides guidelines for using the Rack Air Containment System (RACS) with these units. Additional information regarding RACS with InRow units can be found in Application Note AN-90.
PDF
(rev. 0)
-
ACRP Requirements for Selecting 3rd Party Remote Air-Cooled Condenser and Flooded Receiver -
The InfraStruXure InRow RP (ACRP100, ACRP101, and ACRP102) is an air-cooled DX air conditioner for data centers. All air-cooled air conditioners require the use of remote air-cooled condensers. This application note outlines the requirements for selecting third party remote condenser and flooded receiver for InRow RP air-cooled product.
PDF
(rev. 0)
-
InRow RP-CW and InRow RP-DX Environmental Control -
The InRow RP controls the environment with four basic functions: cool, reheat, dehumidification, and humidification and various combinations thereof. This application note describes the control process for the InRow RP. In order to provide environmental control, the InRow RP units monitor the temperature and humidity of the return air, temperature and humidity of the supply air, and three remote rack inlet temperatures.
PDF
(rev. 0)
-
Data Center Humidification Strategies -
ASHRAE recommends maintaining relative humidity in the range of 40-55% at the air inlet of critical data center IT equipment. This application note first considers various methods of quantifying the expected humidification and dehumidification loads for this design humidity range. After determining latent loading, an approach to equipment selection is offered using APC-MGE InRow products; IR-RC, IR-RP and the FM product as an example.
PDF
(rev. 0)
-
Practices for Pressure Relief Valve Discharge Piping -
Many mechanical refrigeration systems containing large quantities of refrigerant possess pressure relief devices. Under certain conditions, these systems are piped to the outdoors to prevent the displacement of air inside a structure. This paper is intended to give a list of best practices for sizing the piping from the discharge of a pressure relief valve to the outside.
PDF
(rev. 0)
-
ACRP Remote Air-Cooled Condenser Application and Placement -
The InfraStruXure InRow RP (ACRP100, ACRP101, and ACRP102) is an air-cooled DX air conditioner for data centers. All air-cooled air conditioners require the use of remote air-cooled condensers. This application note outlines the placement, refrigerant line pipe sizing, and maintenance of air-cooled condensers for the ACRP100 series units.
PDF
(rev. 0)
-
Using MCA and MOP Ratings to Safely Connect Your Field Wired Air Conditioner -
The minimum circuit ampacity (MCA) and maximum overcurrent protection (MOP) ratings provide guidance for safely connecting field-wired equipment to the building mains in North America. Understanding these ratings, and their relationship to each other, is critical to properly selecting wire and circuit breaker sizes.
PDF
(rev. 0)
-
Pump Selection for InRow Glycol-Cooled Unit System ACRD20X -
While pump packages are not directly supported from APC, a minimal design effort is required for the installer to select the necessary components to design and build the pump package for the condenser water / glycol mixture loop. This application note provides the installing contractor with necessary information regarding part selection and design for pump package needed for operation of the water / glycol mixture loop.
PDF
(rev. 0)
Brochure
Design/Configuration
-
Guide Spec
-
-
InRow RD Guide Specifications -
CSI formatted guide specifications for the InRow RD
PDF
(rev. 0)
-
InfraStruXure InRow RP Guide Specifications -
CSI formatted guide specifications for the InRow RP
ZIP
(rev. 0)
-
InRow RD Guide Specifications -
CSI formatted guide specifications for the InRow RD
ZIP
(rev. 0)
-
Submittal Drawing
-
-
ACRP100-101 - InRow RP DX Air cooled -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RP
PDF
(rev. 4)
-
ACCD75201-75206 - InRow RP DX, Condensers -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RP
PDF
(rev. 1)
-
ACRD500-501 - InRow RD, 600mm, Air Cooled -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RD
PDF
(rev. 1)
-
ACRD100-101 - InRow-RD, Air Cooled -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RD
PDF
(rev. 1)
-
ACRD200-201 - InRow RD, Fluid Cooled -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RD
PDF
(rev. 0)
-
ACAC75009 - Flooded Receiver, 17lb, R410A, ø6" O.D. x 18" -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RD
PDF
(rev. 0)
-
ACFC75255-75210 - Fluid cooler, Single Circuit,480V,3PH,60Hz -
InfraStruXure, NetworkAir Product, InfraStruXure InRow RD
PDF
(rev. 0)
-
User Manual
-
-
InfraStruXure InRow RP Tech Data (Manual) -
General Specifications; Technical Specifications; Bid Specifications
PDF
(rev. 2)
-
InRow RD 10kW Air Cooled Installation -
Installation manual for InRow RD 10kW
PDF
(rev. 2)
-
InRow RD 10kW Fluid Cooled Installation -
Installation manual for InRow RD 10kW
PDF
(rev. 2)
-
InRow RD Technical Data Manual -
Provide pre-sales information for the ACRD units.
PDF
(rev. 2)
-
InfraStruXure InRow RP DX (Manual) -
Operation
PDF
(rev. 1)
-
InRow RP Installation -
Instructions for installing the unit to a prepared location.
PDF
(rev. 1)
-
InRow Cooling Unit Unpacking Sheet -
Unpack all InRow products
PDF
(rev. 1)
-
Installation Instructions - Isolation Valves -
How to install isolation valves to the air-cooled 10kw
PDF
(rev. 1)
-
InRow RD Fluid Cooled Operation and Maintenance -
Operation, Maintenance, and Troubleshooting instructions
PDF
(rev. 1)
-
InRow RD Operation and Maintenance -
Operation, Maintenance and Troubleshooting
PDF
(rev. 1)
-
InRow Full Rack RD Installation -
Covers the RPDX without reheat and humidification.
PDF
(rev. 0)
-
InRow RD Air Cooled Operation and Maintenance -
Operation, Maintenance, and Troubleshooting instructions
PDF
(rev. 0)
-
InRow RP/RC/RD (600mm) Online Guide -
Online User's Guide
PDF
(rev. 0)
Disclaimer: Information at this site is provided solely for the user's information and, while thought to be accurate, is provided strictly "as is" and without warranty of any kind. APC, its agents, employees or contractors will not be liable to you for any damages, direct or indirect, or lost profits arising out of your use of information provided at this site, or information provided at any other site that can be accessed from this site. Unauthorized attempts to upload information or change information on this website are strictly prohibited and may be punishable under the Computer Fraud and Abuse Act of 1986 and the National Information Infrastructure Protection Act. Information may also be used for authorized law enforcement investigations. Copyright © 2009 APC, All rights reserved.