Loading...

Engineering Designer Guide

Configurable Power Accessories
APC’s power distribution accessories deliver the flexibility and management that data centers require. By providing a comprehensive selection of single- and three-phase whips, breakers, connector... [read more]
App Note
  • Using APC InfraStruXure Three Phase Whips and RM PDUs for Non-linear Loads - Consulting Engineers and customers frequently express concern about the acceptability of three phase, 4-wire whips and rack-mount PDUs that are used to distribute InfraStruXure power in a nonlinear load environment. APC is frequently challenged to supply 200% rated neutral conductors. APC conducted extensive testing and demonstrated beyond any doubt that the whips and rack-mount PDUs can be safely used in the worst nonlinear load environment. This application note describes the test methods and provides the test results that support that conclusion. PDF PDF (rev. 2)  
  • Configuring Data Centers to Support HP BladeSystem p-Class Servers - HP BladeSystem p-Class servers operate at a power density 10X higher than that of a typical data center, which demands special attention to the power and cooling system. Success in deploying these servers – there are five basic strategies – requires an understanding of several inputs, including the business needs driving the deployment, user preferences, blade requirements, and constraints. This Application Note considers these inputs, and guides the reader to (1)select the best deployment method from the five basic methods, (2) choose the appropriate rack, cooling, power, and management solutions, and (3) apply these solutions to fit individual needs. PDF PDF (rev. 1)  
Brochure
  • InfraStruXure® Modular Power Distribution 480:415V Power Distribution Unit 400V Remote Power Panel - High Performance 3 Phase Modular, Scalable Power Distribution with Industry Leading Efficiency, Capacity and Performance for Medium to Large Data Centers and Mission Critical Environments PDF PDF (rev. 0)  
Design/Configuration
Guide Spec
Submittal Drawing
User Manual
Configurable Power Distribution
Increase availability in your data center with real-time branch current monitoring and threshold settings for local and advanced, remote notification. The configure-to-order (CTO) process allows for... [read more]
App Note
  • InfraStruXure Agency Listings - This paper describes the Safety Agency testing and certification that has been done on APC's InfraStruXure line of power and air conditioning products. It explains the thought process behind why a particular standard applies to the product. It also explains the benefits of such testing, in particular when electrical inspectors may have concerns about the acceptability of ISX under local codes. Tables list the various models of power and air products and their corresponding domestic and international safety agency listings. PDF PDF (rev. 4)  
  • Access Floor Loading for InfraStruXure Type B - This application note provides basic information about access floor (raised floor) loading and what must be done when installing an APC InfraStruXure Type B solution PDF PDF (rev. 3)  
  • Using APC InfraStruXure Three Phase Whips and RM PDUs for Non-linear Loads - Consulting Engineers and customers frequently express concern about the acceptability of three phase, 4-wire whips and rack-mount PDUs that are used to distribute InfraStruXure power in a nonlinear load environment. APC is frequently challenged to supply 200% rated neutral conductors. APC conducted extensive testing and demonstrated beyond any doubt that the whips and rack-mount PDUs can be safely used in the worst nonlinear load environment. This application note describes the test methods and provides the test results that support that conclusion. PDF PDF (rev. 2)  
  • Configuration of InfraStruXure for Data Centers to Support Dell PowerEdge 1855 Blade Servers - The Introdcution of blade servers has created many challenges for those who design and support NCPI. InfraStruXure for Data Centers can be configured to meet the dynamic needs of Dell PowerEdge 1855 Blade Servers PDF PDF (rev. 1)  
  • APC Symmetra® PX 40K UPS Frame Installation Deviation and Selection of Input Circuit Breaker Ratings - The APC Symmetra® PX scalable UPS frames provide customers with unique UPS power level scalability. This document gives the specifications for permitted input circuit breaker sizes for use with the APC Symmetra PX 40K scalable UPS frame and a 208Y/120V, 60 Hz utility source. This Applications Note is applicable to only the following APC SKU’s: SY10K40F , SY20K40F, SY30K40F, SY40K40F, when configured as either standalone systems or with the InfraStruXure® PDU 40kW 208V/208V W/ MBPwD w/o transformer - PDRPPNX10-M. This Applications Note does not apply to any configuration that includes the following APC InfraStruXure® PDU w/ MBPwD SKU’s which include input isolation transformers: PD40F6FK1-M or PD40G6FK1-M or PD40L6FK1-M PDF PDF (rev. 0)  
  • APC Symmetra® PX 80K UPS Frame Installation Deviation and Selection of Input Circuit Breaker Ratings - The APC Symmetra® PX scalable UPS frames provide customers with unique UPS power level scalability. This document gives the specifications for permitted input circuit breaker sizes for use with the APC Symmetra PX 80K scalable UPS frame and a 208Y/120V, 60 Hz utility source. This Applications Note is applicable to only the following APC SKU’s: SY10K80F, SY20K80F, SY30K80F, SY40K80F, SY50K80F, SY60K80F, SY70K80F, and SY80K80F when configured as either standalone systems or with the InfraStruXure® PDU 40kW 208V/208V W/ MBP w/o transformer PDRPPNX14-M. This Applications Note does not apply to any configuration that includes the following APC InfraStruXure® PDU w/MBP SKU’s which include an input isolation transformer: PD80F6FK1-M or PD80G6FK1-M or PD80L6FK1-M. PDF PDF (rev. 0)  
Brochure
  • InfraStruXure® Modular Power Distribution 480:415V Power Distribution Unit 400V Remote Power Panel - High Performance 3 Phase Modular, Scalable Power Distribution with Industry Leading Efficiency, Capacity and Performance for Medium to Large Data Centers and Mission Critical Environments PDF PDF (rev. 0)  
Design/Configuration
Guide Spec
  • Guide Specification for ISX 150kW PDU - Offer the ability for our customers to build their design standards around APC's ISX 150kW PDU ZIP ZIP (rev. 0)  
Submittal Drawing
  • ISX-PDU40F1XF-5L - PDU 208V Five Line w XFMR - InfraStruXure, ISX 40kW, 208V Input, With Transformer, PDU 40kW with MBP PDF PDF (rev. 4)  
  • ISX-PDU80F1XF - PDU 208V Input Single feed - InfraStruXure, ISX 80kW, 208V Input, PDU 80kW with MBP, Single Feed, With Transformer PDF PDF (rev. 4)  
  • ISX-PDU80F1XF-5L - PDU 208V Input Single feed 5L - InfraStruXure, ISX 80kW, 208V Input, PDU 80kW with MBP, Single Feed, With Transformer PDF PDF (rev. 4)  
  • ISX-PDU80G1XF - PDU 480V Input Single feed - InfraStruXure, ISX 80kW, 480V Input, PDU 80kW with MBP, Single Feed, With Transformer PDF PDF (rev. 4)  
  • ISX-PDU80G1XF-5L - PDU 480V Input Single feed 5L - InfraStruXure, ISX 80kW, 480V Input, PDU 80kW with MBP, Single Feed, With Transformer PDF PDF (rev. 4)  
  • ISX-PDU80G2XF-5L - PDU 480V Input Dual feed 5L - InfraStruXure, ISX 80kW, 480V Input, PDU 80kW with MBP, Dual Feed, With Transformer PDF PDF (rev. 4)  
  • ISX-PDU80L1XF-5L - PDU 600V Input Single feed 5L - InfraStruXure, ISX 80kW, 600V Input, PDU 80kW with MBP, Single Feed, With Transformer PDF PDF (rev. 4)  
  • ISX-PDU40G1XF-5L - PDU 480V Input Five Line w XFMR - InfraStruXure, ISX 40kW, 480V Input, PDU 40kW with MBP PDF PDF (rev. 4)  
  • ISX-PDU40F1NXF-5L - PDU 208V Five Line wo XFMR - InfraStruXure, ISX 40kW, 208V Input, Without Transformer, PDU 40kW with MBP PDF PDF (rev. 3)  
  • ISX-PDU80F1NXF - PDU 208V Input Single feed - InfraStruXure, ISX 80kW, 208V Input, PDU 80kW with MBP, Single Feed, Without Transformer PDF PDF (rev. 3)  
  • ISX-PDU80F2NXF - PDU 208V Input Dual feed - InfraStruXure, ISX 80kW, 208V Input, PDU 80kW with MBP, Dual Feed, Without Transformer PDF PDF (rev. 3)  
  • ISX-PDU80F2NXF-5L - PDU 208V Input Dual feed 5L - InfraStruXure, ISX 80kW, 208V Input, PDU 80kW with MBP, Dual Feed, Without Transformer PDF PDF (rev. 3)  
  • ISX-PDU80F2XF - PDU 208V Input Dual feed - InfraStruXure, ISX 80kW, 208V Input, PDU 80kW with MBP, Dual Feed, With Transformer PDF PDF (rev. 3)  
  • ISX-PDU80F2XF-5L - PDU 208V Input Dual feed 5L - InfraStruXure, ISX 80kW, 208V Input, PDU 80kW with MBP, Dual Feed, With Transformer PDF PDF (rev. 3)  
  • ISX-PDU80G2XF - PDU 480V Input Dual feed - InfraStruXure, ISX 80kW, 480V Input, PDU 80kW with MBP, Dual Feed, With Transformer PDF PDF (rev. 3)  
  • ISX-PDU80L2XF-5L - PDU 600V Input Dual feed 5L - InfraStruXure, ISX 80kW, 600V Input, PDU 80kW with MBP, Dual Feed, With Transformer PDF PDF (rev. 3)  
  • ISX-PDU40L1XF-5L - PDU 600V Input Five Line w XFMR - InfraStruXure, ISX 40kW, 600V Input, PDU 40kW with MBP PDF PDF (rev. 3)  
  • ISX-PD150G6F - PDU 150kW 480V Input Full set of drawings - InfraStruXure, ISX 150kW PDU, 480V Input PDF PDF (rev. 3)  
  • ISX-PD60FF-5L - PDU 208V Input Five Line w XFMR - InfraStruXure, ISX 60kW PDU, 208V Input PDF PDF (rev. 3)  
  • ISX-PD60GF-5L - PDU 480V Input Five Line w XFMR - InfraStruXure, ISX 60kW PDU, 480V Input PDF PDF (rev. 3)  
  • ISX-PD60LF-5L - PDU 600V Input Five Line w XFMR - InfraStruXure, ISX 60kW PDU, 600V Input PDF PDF (rev. 3)  
  • ISX-PDU40F1XF - PDU 208V w XFMR - InfraStruXure, ISX 40kW, 208V Input, With Transformer, PDU 40kW with MBP PDF PDF (rev. 2)  
  • ISX-PDU40F1NXF - PDU 208V wo XFMR - InfraStruXure, ISX 40kW, 208V Input, Without Transformer, PDU 40kW with MBP PDF PDF (rev. 2)  
  • ISX-PDU80F1NXF-5L - PDU 208V Input Single feed 5L - InfraStruXure, ISX 80kW, 208V Input, PDU 80kW with MBP, Single Feed, Without Transformer PDF PDF (rev. 2)  
  • ISX-PDU80L1XF - PDU 600V Input Single feed - InfraStruXure, ISX 80kW, 600V Input, PDU 80kW with MBP, Single Feed, With Transformer PDF PDF (rev. 2)  
  • ISX-PDU80L2XF - PDU 600V Input Dual feed - InfraStruXure, ISX 80kW, 600V Input, PDU 80kW with MBP, Dual Feed, With Transformer PDF PDF (rev. 2)  
  • ISX-PDU40G1XF - PDU 480V Input w XFMR - InfraStruXure, ISX 40kW, 480V Input, PDU 40kW with MBP PDF PDF (rev. 2)  
  • ISX-PDU40L1XF - PDU 600V Input w XFMR - InfraStruXure, ISX 40kW, 600V Input, PDU 40kW with MBP PDF PDF (rev. 2)  
  • ISX-PD150G6F-5L - PDU 150kW 480V Input 5L Diagram - InfraStruXure, ISX 150kW PDU, 480V Input PDF PDF (rev. 2)  
  • ISX-PD60FF - PDU 208V Input w XFMR - InfraStruXure, ISX 60kW PDU, 208V Input PDF PDF (rev. 1)  
  • ISX-PD60GF - PDU 480V Input w XFMR - InfraStruXure, ISX 60kW PDU, 480V Input PDF PDF (rev. 1)  
  • ISX-PD60LF - PDU 600V Input w XFMR - InfraStruXure, ISX 60kW PDU, 600V Input PDF PDF (rev. 1)  
  • ISX-PDRPP - Distribution Panel w Isolated Gnd - InfraStruXure, ISX 60kW PDU, PDRPP PDF PDF (rev. 1)  
  • ISX-PDRPP-ES - Distribution Panel w Isolated Gnd, Electrical Schematic - InfraStruXure, ISX 60kW PDU, PDRPP PDF PDF (rev. 1)  
  • ISX-PDU40K - PDU (40-60)kW, 208V or 480V or 600V, Floor Anchoring - InfraStruXure, ISX 40kW, Floor Anchoring PDF PDF (rev. 1)  
  • PDRDPF10U-208V Rack Distribution Panel Mounted in SX Rack - Configurable Power Distribution, Rack Distribution Panel 208 V PDF PDF (rev. 0)  
  • ISX-PDU80K - PDU 80kVA, 208V or 480V or 600V, Floor Anchoring - InfraStruXure, ISX 80kW, Floor Anchoring PDF PDF (rev. 0)  
  • ISX-PDU80KX - PDU 80kW with Transformer (208V or 480V or 600V) - InfraStruXure, ISX 80kW, Center of Gravity PDF PDF (rev. 0)  
User Manual
  • InfraStruXure Power Distribution Units (Online Guide) - Configuration PDF PDF (rev. 1)  
  • InfraStruXure Power Distribution Units Panel Board Schedule 230 V, 400 V (Sheet) - Panel board schedule for InfraStruXure PDU circuit breaker panels (230/400V). PDF PDF (rev. 0)  
  • PDF PDF (rev. 0)  
  • PDF PDF (rev. 0)  
  • PDF PDF (rev. 0)  
  • PDF PDF (rev. 0)  
  • PDF PDF (rev. 0)  
  • PDF PDF (rev. 0)  
  • PDF PDF (rev. 0)  
  • PDF PDF (rev. 0)  
  • PDF PDF (rev. 0)  
  • PDF PDF (rev. 0)  
  • PDF PDF (rev. 0)  
MGE Service Bypass (testing Phrase)
External Maintenance By-pass is available in either a stand alone or wall mount cabinet for increased safety during service and preventative maintenance. These cabinets allow for a full wrap around... [read more]
App Note
Brochure
Design/Configuration
Guide Spec
Submittal Drawing
User Manual
  • MGE Galaxy 4000 40-75kVA Installation and User Manual - MGE Galaxy 4000 40-75kVA Installation and User Manual PDF PDF (rev. 2)  
MGE Static Transfer Switches (3-Phase 200-600A, 208-600V)
MGE Static Transfer Switches
MGE static transfer switches (STS) supply power to a range of equipment from two independent and redundant sources. Static Transfer Switches automatically transfer power to a stable alternate source... [read more]
App Note
Brochure
  • Brochure for MGE Epsilon STS (NAM) - Brochure for MGE Epsilon STS displaying features and specifications PDF PDF (rev. 0)  
Design/Configuration
Guide Spec
  • Guide Specifications for MGE Epsilon Static Transfer Switch - Guide Specifications for MGE Epsilon Static Transfer Switch. PDF PDF (rev. 0)  
Submittal Drawing
User Manual
  • MGE Epsilon STS Installation and User Manual (200/400/600A) - MGE Epsilon STS Installation and User Manual (200-600A) PDF PDF (rev. 0)  
  • Epsilon STS 200 A/400 A/600 A Static Transfer Switch Installation and User Manual - Installation and User Manual for Epsilon STS 200 A/400 A/600 A Static Transfer Switch PDF PDF (rev. 0)  
Modular Power Accessories
APC Power Distribution Modules simplify both the global deployment of a standard power distribution system and the expansion of existing APC Modular Power Distribution Unit solutions. A variety of... [read more]
App Note
Brochure
  • InfraStruXure® Modular Power Distribution 480:415V Power Distribution Unit 400V Remote Power Panel - High Performance 3 Phase Modular, Scalable Power Distribution with Industry Leading Efficiency, Capacity and Performance for Medium to Large Data Centers and Mission Critical Environments PDF PDF (rev. 0)  
Design/Configuration
Guide Spec
Submittal Drawing
User Manual
  • Module installation and operation of 3 phase Power distribution - Power Distribution Module Installation instructions PDF PDF (rev. 1)  
  • Modular Power Distribution Unit Operation - Operation and maintenance PDF PDF (rev. 0)  
  • IEC309 to 3 x C-19 Connector Cable Installation Sheet - Splitter Cable for Blade Servers Installation Instructions PDF PDF (rev. 0)  
  • Modbus Map RPP/RDP - Modbus Map PDF PDF (rev. 0)  
Modular Power Distribution
Modular Power Distribution mitigates the need to predict the future requirements and configurations of your data center. This visionary power distribution system is agile enough to match the needs... [read more]
App Note
  • InfraStruXure RPP Modular Power Distribution Unit: Hot Aisle Containment Application Guidelines and In Row Baying Instructions - The 300-mm Remote Power Panel (RPP) Modular Power Distribution Unit (MPDU) (Only PDPM277H 400V EMEA/APJ/GCN and PDPM144F 208V NAM) is the power source for Rack Mounted Distribution Units and IT loads. As illustrated in Figure 1, it houses the hot-pluggable power backplane, monitoring bus, controller, Web card and the support structure for the Power Distribution Modules. Specially designed offset brackets ship with the unit to allow joining to other InRow® products and racks in the row or in a Hot Aisle Containment System (HACS) configuration. HACS door frame configurations do not allow the 300-mm RPP to be located at the end of the aisle. PDF PDF (rev. 1)  
Brochure
  • InfraStruXure® Modular Power Distribution 480:415V Power Distribution Unit 400V Remote Power Panel - High Performance 3 Phase Modular, Scalable Power Distribution with Industry Leading Efficiency, Capacity and Performance for Medium to Large Data Centers and Mission Critical Environments PDF PDF (rev. 0)  
Design/Configuration
Guide Spec
Submittal Drawing
  • PDPM288G6H-SD - ISX Modular PDU 266kVA System One Line Diagram - InfraStruXure, ISX Modular PDU 266kW PDF PDF (rev. 0)  
  • PDPM288G6H - ISX PDU 288kW,Auto Transformer,Modular distribution - InfraStruXure, ISX Modular PDU 288kW PDF PDF (rev. 0)  
User Manual
  • InfraStruXure Modular PDU 480 V Installation - This document contains important instructions that should be followed during installation and maintenance of the InfraStruXure Modular Power Distribution Unit (PDU). PDF PDF (rev. 1)  
  • Modular Power Distribution Unit Operation - Operation and maintenance PDF PDF (rev. 0)  
  • InfraStruXure Modular PDU 480 V Unpacking - This document contains important instructions that should be followed during receiving, unpacking, and installation of the InfraStruXure Modular Power Distribution Unit (PDU). PDF PDF (rev. 0)  
  • InfraStruXure Modular PDU 480 V Operation - Operation PDF PDF (rev. 0)  
  • InfraStruXure Modular Rack-Mount Power Distribution in an SX rack - Receiving, Unpacking PDF PDF (rev. 0)  
  • Remote Power Panel (RPP) Modular Power Distribution Unit (415 V) - Installation - Installation Sheet PDF PDF (rev. 0)  
  • Operation Addendum - Modbus Configuration for Modular Distribution - Addition of Modbus capability PDF PDF (rev. 0)  
  • Modbus Map RPP/RDP - Modbus Map PDF PDF (rev. 0)  
  • Modular Distribution RPP/RDP - Release Notes PDF PDF (rev. 0)  
Service Bypass Panel (testing Phrase)
testing Phrase
App Note
Brochure
Design/Configuration
Guide Spec
Submittal Drawing
User Manual
  • Service Bypass Panel Floor MBP with Power 10-30 kVA 208 V (Manual) - Installation; Operation PDF PDF (rev. 0)  
Disclaimer: Information at this site is provided solely for the user's information and, while thought to be accurate, is provided strictly "as is" and without warranty of any kind. APC, its agents, employees or contractors will not be liable to you for any damages, direct or indirect, or lost profits arising out of your use of information provided at this site, or information provided at any other site that can be accessed from this site. Unauthorized attempts to upload information or change information on this website are strictly prohibited and may be punishable under the Computer Fraud and Abuse Act of 1986 and the National Information Infrastructure Protection Act. Information may also be used for authorized law enforcement investigations. Copyright © 2009 APC, All rights reserved.