|
Usted está aquí:
|
A quick quiz to determine your susceptibility to power problems... |
|
| How frequent are brownouts or blackouts? | Risk Factor |
| Chronic - greater than 12 per year | 300 |
| Frequent - greater than 3 per year | 80 |
| Infrequent - less than 3 per year | 50 |
|
Overloaded or poor wiring is a major cause of power problems. Wiring systems in many older buildings were not designed to handle the demands of today's office equipment. |
|
| Building age: | Risk Factor |
| Over ten years | 100 |
| Between 5 and 10 years | 80 |
| Under 5 years | 50 |
|
Underground power distribution suffers fewer problems than pole linked sources, which are subject to the hazards of tree branches, auto accidents, and curious animals. |
|
| Utility supplied by: | Risk Factor |
| Above-ground poles | 100 |
| Underground wiring | 10 |
|
Studies have shown that as much as 50% of power problems can be tied to the local work environment. The innocent looking copy machine or laser printer may be responsible for data loss on your computer. An elevator on the other side of the wall may cause lock-ups every time a courier arrives! |
|
| Office equipment in proximity: | Risk Factor |
| Heavy Machinery / Motors | 200 |
| Copiers / Laser printers | 150 | None | 20 |
|
The same lightning and surge events that cause damaging utility line transients can also cause power problems to reach your equipment through the "back door" on serial, telephone/modem and LAN connections |
|
| Connections to Modem and Peripherals: | Risk Factor |
| Modem, serial, and network connections | 200 |
| Modem connection only | 80 |
| No connection/Stand alone | 50 |
|
Advanced network and multi-tasking operating systems depend on cache memory. |
|
| Operating System: | Risk Factor |
| Network (NetWare, Windows NT) | 100 |
| Stand-alone Multi-tasking (OS/2,Unix,Windows 95) | 80 |
| Stand alone single-tasking (DOS, Windows 3.1) | 50 |
|
As a network or multi-user system grows, the points of susceptibility also increase. The design of a LAN can also influence its susceptibility to power problems, as a cluster-oriented LAN may be unaffected by problems that bring down a LAN on a backbone. |
|
| Size of system: | Risk Factor |
| More than 10 users | 100 |
| Between 5 and 10 users | 80 |
| Less than 5 users | 50 |
|
Rural sites are notorious for bad power. As common sense dictates, the farther power travels, the greater the chance of a disturbance along the way. |
|
| Distance from utility provider: | Risk Factor |
| More than 200 miles | 100 |
| Less than 200 miles | 80 |
|
Lightning is perhaps the most dramatic reminder of the susceptibility of computers to damage and data loss. Lightning and surges go hand in hand with brown-outs and blackouts. (Refer to the picture below to find the average number of lightning storms your area experiences each year) |
|
| Storms per year: | Risk Factor |
| More than 30 | 300 |
| Between 20 and 30 | 100 |
| Less than 20 | 50 |
|
As populations grow and additional generating facilities aren't built, rolling brownouts become a definite reality. (Refer to the picture below to find the estimated percentage Undercapacity of power suppliers in your area) |
|
| Utility demand: | Risk Factor |
| More than 10% Undercapacity | 200 |
| More than 5% Undercapacity | 100 |
| Less than 5% Undercapacity | 80 |
|
After finishing the quiz, click the "Calculate Risk" button below to find your total Risk Factor. |
|