Анонсы продуктов

APC объявляет о*:

1 Записи найдены | Nov-2018 Объявления
Новый продукт

UPS NMC Firmware Update v6.6.4 with BACnet/IP Certification

Firmware Upgrades

UPS NMC Firmware Update v6.6.4 with BACnet/IP support, for smooth integration of UPS with Building Management Systems (BMS), is now certified by BACnet Testing Laboratories (BTL). This certification ensures compatibility with similarly certified 3rd party BACnet Devices and Management Systems. In addition, this firmware update addresses multiple reported issues including, - mitigating ROBOT vulnerability, by providing an option for the users to select active cipher suites, - now able to accept SSL/TLS certificates issued by third party Certificate Authorities such as Microsoft Certificate Services - overcome white screen on web User Interface, due to abnormally large amount of cookies in the web browser. To download the UPS NMC Firmware Update v6.6.4 (for single phase Smart-UPS & Symmetra) SFSUMX664, SFSY664 and language packs, kindly navigate to www.apc.com/tools/download/, "filter by Software/Firmware" and choose "Firmware Upgrades - UPS Network Management Card".

Артикул: SFSUMX664, SFSUMX664LP1, SFSUMX664LP2, SFSY664, SFSY664LP1, SFSY664LP2

* Результаты зависят от выбранной вами страны.