Technical FAQs

Ask a Question

Errors being reported in log file for PowerChute-keystore and it is not present in PowerChute/group1 folder after installation completes.

Issue:
Errors being reported in log file for PowerChute-keystore and it is not present in group1 folder after installation completes.

ERROR main com.apcc.m11.components.StdPowerSource.SecurityCertificateManager - SecurityCertificateManager.checkCertificateInKeystore - tried to fix keystore error:java.security.KeyStoreException: JKS not found
ERROR main com.apcc.m11.components.StdPowerSource.SecurityCertificateManager - PowerChute-keystore (A file or directory in the path name does not exist.)

Product:
PowerChute Network Shutdown version 3.1

Environment:
AIX 7.1

Cause:
IBMJCE provider in combination with Java 7_64

Solution:
This issue has been address in PowerChute Network Shutdown version 4.0 and above
Was this helpful?
What can we do to improve the information ?