Technical FAQs

Ask a Question

FTP Alert Action in Version 2 Appliances is Active Mode Only

Issue:

FTP Alert Action in Version 2 Appliances is Active Mode Only

Product Line:

NetBotz

Environment:

NetBotz version 2 and 3

Cause:

The FTP Alert Action included with the Version 2 Appliances (320, 420, 500) is an Active Mode FTP session only. At this time, NetBotz Appliances do NOT support passive FTP.

Resolution:

This is by design. No alternative options are available.
 
Was this helpful?
What can we do to improve the information ?