Ping Response (ICMP Requests) Can Be Disabled on NetBotz Version 2 Appliances
Issue:
Ping Response (ICMP Requests) Can Be Disabled on NetBotz Version 2 Appliances
Product Line:
NetBotz
Environment:
NetBotz version 2
Cause:
Alternative configurations
Resolution:
It is possible to turn off or disable ICMP responses/requests on NetBotz version 2 Appliances (Models 320, 420, & 500). To do so, you must enable "IP Filter" functionality via the Advanced View. Once IP Filtering is enabled, the bot will only respond to requests (including ICMP requests) from specific IP addresses