Technical FAQs

Ask a Question

DCO | Can more than one client instance be running on the same computer?

Issue:
Can more than one (1) instance of a Data Center Operation desktop client be used on a computer at the same time?

Product Line:
StruxureWare Data Center Operation (DCO)

Environment:
StruxureWare Data Center Operation (all versions)

Cause:
When attempting to load more than one DCO desktop client on the same computer an error message appears displaying, "There is another application instance started by the current user and the workspace directory is currently in use."

Resolution:

Only one instance of the DCO Desktop Client can be opened at a time.  This is by design and there is no work around for opening more than one client on the same computer at the same time.
Was this helpful?
What can we do to improve the information ?