Technical FAQs

Ask a Question

Can AR8008BLK or AR8016ABLK be used in the NetShelter Networking cabinets?

Issue:
The NetShelter SX Networking cabinets have open mounting rails which do not support the cable side channels.

Product Line:
NetShelter SX Networking

Environment:
All versions and serial ranges.

Cause:
A customer needs to run cables from front to rear in a NetShelter SX Networking cabinet.

Resolution:
In the Networking cabinets you can use horizontal cable managers to connect the side channels from front to rear. A typical setup would be to have AR8603A or AR8428 installed on the front and rear mounting rails, and run AR8008BLK or AR8016ABLK between them.
Was this helpful?
What can we do to improve the information ?