Technical FAQs

Ask a Question

PowerChute Network Shutdown fails to run command file on HP-UX

Run command file fails to work when an event is triggered.


PowerChute Network Shutdown versions 3.0.1, 3.1


HP-UX 11iv3


Install PowerChute and configure in Single mode. Configure command file for on battery in the configure event page. Also configure command file in the shutdown settings page. Generate on battery event.

Expected Result: Command file should run

Actual Result: Failed to run the command file

Upgrade to PowerChute Network Shutdown version 4.x

Was this helpful?
What can we do to improve the information ?