Technical FAQs

Ask a Question

Are there baying brackets available for the NetShelter VX Seismic cabinets?

Issue:
Customers may want to bay together NetShelter VX Seismic cabinets.

Product Line:
NetShelter VX Seismic
 
Environment:
All versions and date ranges.

Cause:
Customers may want to use baying brackets to enhance the seismic feature, or to help align rows of cabinets.
 
Resolution:
There are no baying brackets for the NetShelter VX Seismic cabinets.
The NetShelter VX Seismic cabinets are designed to be mounted to the floor in NEBS GR-63-CORE seismic installations, and baying brackets are not necessary. Baying brackets do not enhance the seismic feature of the cabinet.
Was this helpful?
What can we do to improve the information ?