Technical FAQs

Ask a Question

Why is my APC Back-UPS giving a single beep every 5 seconds?


Why is my APC Back-UPS emiting a single beep every 5 seconds?

Product Line:

Back-UPS, Back-UPS PRO




The Back-UPS product has transferred to battery power due to a low voltage condition at the wall. The Back-UPS has remained Onbattery until its runtime was totally exhausted, however, there was still enough voltage present at the wall to trickle charge the battery.


This is considered to be a normal operating state.

When the voltage returns to normal the Back-UPS will wake up and restore power to the battery outlets.
Was this helpful?
What can we do to improve the information ?