Technical FAQs

Ask a Question

Physical Sizes of Camera Pod 120 and Sensor Pod 120

Issue:

Physical Sizes of Camera Pod 120 and Sensor Pod 120

Product Line:

NetBotz

Environment:

NetBotz Version 2 camera pod NBPD0121

Cause:

Physical size

Resolution:

Physical Sizes of Camera Pod 120 and Sensor Pod 120

Camera Pod 120
Height (counting jacks on top) = 2.783
Height (not counting jacks on top) = 2.70
Width = 2.625
Depth = 1.090


Sensor Pod 120
Height = 3.863
Width (including temp sensor on the side) = 2.930
Width (not including temp sensor on side) = 2.612
Depth = 1.10

NOTE: The USB cable usually sticks out of the side of the pods about 2 inches.
 
Was this helpful?
What can we do to improve the information ?