Technical FAQs

Ask a Question

How Do I Eliminate Multiple Alert Notifications

Issue:

Eliminating Multiple Alert Notifications from NetBotz appliances

Product Line:

NetBotz

Environment:

Potentially any version

Cause:

Potentially, different configuration options may cause repeated alerts.

Resolution:

- Check that each alert action associated with an alert sequence does not have duplicate addresses associated with it.
- Verify that the different alert sequences within a profile is not set up with the same notifications.
- Thresholds may have a threshold specific e-mail address associated with it. Make sure this is not a duplicate of an address already associated with the actions.
- Make sure the threshold is not set up so that the threshold itself is switching into and out of alert too frequently.
- Increase the notification interval or decrease the number of notifications in the Alert configuration / profile
- Maks sure the check box is unchecked for"Automatically ass new alert actions to this schedule" for any alert profile sequences.
 
Was this helpful?
What can we do to improve the information ?