Video: How to configure PowerChute Network Shutdown to start the shutdown process once the UPS has been running on battery for a specified time?
Issue:
Would like PowerChute Network Shutdown to begin the shutdown process once the UPS has run on battery for pre-determined amount of time.
Product Line:
PowerChute Network Shutdown
Environment:
All supported OS
Cause:
UPS on battery
Resolution:
Log into PowerChute web interface by entering the systems IP address or FQDN on port 6547. Examples https://192.168.1.10:6547 or https://MYComputer@myOffice.com:6547
Go to Configure Events
Select UPS On Battery and click Shutdown
Click Enable Shutdown
Enter the desired amount of time you would like the UPS to run on battery prior to PowerChute starting the shutdown process and then click Apply.
For assistance installing PowerChute Network Shutdown see FAQ FA250921 "How to install PowerChute Network Shutdown 4.x" FAQ FA296461 "How to install and deploy PowerChute Network Shutdown virtual appliance onto VMware" FAQ FA313604 "How to install PowerChute Network Shutdown on VMware vSphere Management Assistant (vMA)"