Technical FAQs

Ask a Question

StruxureWare DCE virtual machine may hang, logs show E1000 NIC error

StruxureWare DCE virtual machine may hang, messages log show E1000 NIC error

Product Line:
StruxureWare Data Center Expert

StruxureWare DCE virtual machine potentially any version.

Potential incompatibility with older Virtual Machine NIC driver.

Looking at DCE log files on a VM install, you may see an error similar to the following: kernel:

e1000 0000:02:00.0: eth0: Detected Tx Unit Hang

This has been seen in VMware ESXi 5.0. It appears to be most prevalent when attempting a DCE backup. In cases where this issue does exist, an upgrade of the VM host to ESXi 5.5 has been seen to resolve this error.
Was this helpful?
What can we do to improve the information ?