Technical FAQs

Ask a Question

Is the root password available for StruxureWare Data Center Expert?

Issue:

What is the root password available for StruxureWare Data Center Expert.

Product Line:

InfraStruxure Central
StruxureWare Data Center Expert

Environment:

Internal systems in StruxureWare

Cause:

StruxureWare uses a customized version of Linux. Older systems ran Fedora Core while the newest versions run Centos. As with any Linux systems a super user or root user has full access to the internal systems and processes.

Resolution:

Because the system is customized, APC and Schneider Electric do not allow customers access to the back end of the system. StruxureWare Data Center Expert is an appliance and should be considered a "black box" or closed system. We do not provide the root password for theses systems.

Was this helpful?
What can we do to improve the information ?