Technical FAQs

Ask a Question

Can the NetShelter CX integral PDU be replaced, or can another be added if a dual power input is required for redundancy?

Issue:
Need an additional or replacement PDU in the NetShelter CX.

Product Line:
NetShelter CX
 
Environment:
All versions and serial ranges.
 
Cause:
Additional PDU or replacement necessary
 
Resolution:
Yes, the PDU can be replaced or others can be added.
The original PDU included with the cabinet is the APC part number AP9568 for EMEA cabinets (50Hz), and AP9567 for  NEMA cabinets (60Hz).
 
Was this helpful?
What can we do to improve the information ?