Technical FAQs

Ask a Question

How humidity threshold alarms are reported on an ACRP

Issue:

How humidity threshold alarms are reported on an ACRP

 

Product line:

ACRP5XX, ACRP1XX, Uniflair, Network Air FM, ACFM, IR40, InRoom

 

Environment:

All Product models, all serial numbers

 

Cause:

Units use dew point to calculate humidity

 

Resolution:

You may come across an ACRP not generating an alarm message when the Return Humidity is lower than the Threshold [figure 1].  Remember Humidity set points and thresholds are based on dew point.  It is possible to be under the RH% set point/threshold and not receive a humidity demand or warning.

 

 

Figure 1

 

 

Was this helpful?
What can we do to improve the information ?