Technical FAQs

Ask a Question

What is the Frequency Range for Network FM fan blowers




Issue:

What is the Frequency Range for Network FM fan blowers

                                                 

Product line:

Network Air FM CRAC Units

 

Environment:

Data Center Room coolers

 

Cause:

Informational the settings below are recommended settings for each size model unit

 

Resolution:

FM35 - 35hz

FM40 - 40hz

FM50 – 48-52 hz

 

Was this helpful?
What can we do to improve the information ?