Technical FAQs

Ask a Question

Leakage current from APC Back UPS products

Issue:

How can I gauge the amount of leakage current from my Back-UPS?

Product Line:

All Back-UPS models.

Environment:

N/A

Cause / Resolution:

All APC Back UPS models, by themselves exhibit less than 1 milli-amps of

leakage current. If a load is attached, then the leakage current measured

on the output of the UPS will include the leakage current of the load as well

as the UPS.
 
Was this helpful?
What can we do to improve the information ?