Are there Gender Changers that have opposite genders, like DB25 male/female?
Issue:
There may be need for an adapter that has a male connector on one end and a female connector on the other.
Product Line:
Cables and Connectivity Solutions
Environment:
All versions and serial ranges.
Cause:
These help lengthen the life expectancy of a port that experiences a high rate of connecting and disconnecting cables.
Resolution:
Yes but they are not really Gender Changers. They are typically called Port Protectors or Port Extenders. They can be used to help lengthen the life expectancy of a port that is repeatedly connected to. They can also be used to add height to a recessed port.
All APC brand Cables and Connectivity Solutions products like Cat 5E, Cat 6, Cat 6A patch cables, fiber optic cables, USB cables and adapters, Monitor cables, A/V cables, adapters and converters can be found at: www.apccables.com