Technical FAQs

Ask a Question

ISX Central 6.2 release notes incorrectly quotes support for Red Hat Linux 6.

Issue:

ISX Central 6.2 release notes incorrectly quotes support for Red Hat Linux 6

Product Line:

InfraStruxure Central

Environment:

InfraStruxure Central 6.2 release notes

Cause:

TIncorrect documentation.

Resolution:

The release notes for ISX Central 6.2 incorrectly list support for Red Hat Linux version 5 and higher. Red Hat 5 has indeed been tested but Red Hat 6 has not. This will be corrected in the next revision of the release notes with the next Central release..

Was this helpful?
What can we do to improve the information ?