Technical FAQs

Ask a Question

Supported PCMCIA Modem Cards for WallBotz 500

Issue:

Supported PCMCIA Modem Cards for WallBotz 500

Product Line:

NetBotz

Environment:

NetBotz 500

Cause:

Supported Accessories

Resolution:

The part number (from Intel) for the only 500-supported modem pc card is CM-56G:
http://www.intel.com/network/connectivity/emea/eng/products/xircm56g.htm


There are some combo cards (10/100 Ethernet + modem) with similar names (i.e. Xircom CreditCard xxxxxxx), and they are NOT supported by WallBotz500.
Was this helpful?
What can we do to improve the information ?