SYRIAN ARAB REPUBLIC - Choose Country or Region
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
SYRIAN ARAB REPUBLIC - Choose Country or Region
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
Particle Sensor 120 Specifications
Issue:
Particle Sensor 120 Specifications
Product Line:
NetBotz
Environment:
NetBotz particle sensor NBES0201
Cause:
Sensor specifications.
Resolution:
Particle Sensor Specifications
Measures presence of dust, *smoke, or other particulates in sensitive equipment spaces
Measures particle concentrations as small as 1 micron
Set thresholds on particulate levels, graph past sensor readings
* please note this unit is not meant to be used as a smoke detector.
Placement
On floor near equipment or mount on wall
Particulates most dense at lower heights, so place as low as possible
Other
Periodic lens cleaning required
Supported on WallBotz 500 onlyConnects to DIN connector on WallBotz 500 Sensor Pod