The image orientation can be altered on all appliances. Simply check the box under Camera Configuration that says ""Rotate Camera Image"". This will rotate the image 180 degrees to allow a camera that is mounted upside down to be displayed properly in the Advanced View or Basic View.