Avoiding False External Temperature Reading in RF Environments on Netbotz Appliances
Issue:
Avoiding False External Temperature Reading in RF Environments on Netbotz Appliances
Product Line:
NetBotz
Environment:
NetBotz version 2.
Cause:
In an environment where strong radio frequency may be introduced, users can try any of the following to eliminate false low temperature readings:
Resolution:
* RF ground the Bot/pod to earth
* RF ground the DIN SHIELD to earth at each of the connector
* Locate a BOT or POD closer to the place where they want to measure and eliminate any extension cable
* Wind the cable (close to the Bot) through a toroidal ferrite several times
* Place the cable in metal, earth grounded conduit to provide a faraday cage