Technical FAQs
Technical FAQs
The location of these stickers varies per Symmetra model:
Symmetra Power Array: bottom, front of UPS. SYMSTRF, SYMINIF, etc.
Symmetra RM 6kVA: front above System Enable switch behind display bezel, or rear bottom-left corner. SYHF6KT
Symmetra RM 12kVA: rear, bottom-right corner. SYPF12KT
Symmetra LX: rear, upper center on UL/Certification Sticker. SYAFxxxx
For Symmetra LX, the model number of the chassis will always begin with "SYAF". It is possible to find a second "configuration" sticker with part # such as SYA12K16RMP located under the System Enable/EPO panel.
Please Note: The Serial Number provided via the PowerView is that of the PowerView display itself. The serial number and manufacturing date provided via the Network Management Card refers to Symmetra Main Intelligence Module that is in control of the UPS.