Technical FAQs

Ask a Question

What are the Condensate Pump lift specifications for your InRow product line?

Issue:
What are the Condensate Pump lift specifications for your InRow product line?
 
Product line:
All InRow Units
 
Environment:
Data Center Cooling
 
Cause:
 
Resolution:
All of the InRow products come with a factory-installed condensate pump piped internally to the condensate pan. Each pump has different specifications.  If needed, more details can be found in the technical manual as well.

InRow ACSC100, ACSC101, ACRD100, ACRD200, ACRC100, ACRC103
Pacific Electronic: Capable of pumping 1.3 GPH (5 L/h)
InRow SC, RD (300mm):
  • Charles Austen Pump - Capable of pumping 13.5 GPH (51 L/h) liquid a maximum distance of  65ft (20m) , which may include a maximum lift of 20 ft (7 m).*
  • Pacific Electronic - Capable of pumping 1.3 GPH (5 L/h) liquid a maximum distance of  50 ft (15.2 m), which may include a maximum lift of 16 ft (4.9 m).
NOTE: Dual floats are included with the unit. One float is used for condensate pump control, the other to generate condensate pan overflow alarms.

ACRP50x, ACRP10x, ACRD50x, ACRC50x, ACRD60x, ACRD60xP
  • Hartell - Capable of pumping 8.45 GPH (0.53 L/m) liquid a maximum distance of 18 m (60 ft), which may include a maximum lift of 11.5ft (3.5 m).
*except for ACRC100 and ACRC103
x = denotes the voltage is for 208v or 460v
Was this helpful?
What can we do to improve the information ?