Technical FAQs
Technical FAQs
For all Smart-UPS products 10Kva or less:
The minimum depth for the rails is 21.75" and the maximum depth is 36".
NOTE: If your Smart-UPS is equipped with cleats (metal pieces attached to the sides of the Smart-UPS chassis that slide into the rails) the minimum depth is 29"".
For Smart-UPS products over than 10Kva:
The minimum depth for the rails is 27.5" and the maximum depth is 33".
If you are using your APC rail kit to mount non-APC equipment your experience may vary.
Please note that some networking specific or custom enclosures may need to be adjusted to accommodate the depth of the rails.