A comprehensive service to assess the power quality and availability of the electrical infrastructure supporting a network environment.

APC will perform a yearly re-inspection of the site with an empasis on ensuring the customer still has the required capacity with their UPS system and that any changes to the site are documented. This re-inspection will include an examination of any changes in the infrastructure from the previous year.

PowerAudit Yearly Review
Benefits to Customer:
  • APC consultants can provide a power expansion plan for the customer
  • Deliverable report to file for reference
  • Increases availability of the electrical infrastructure supporting networking environments
  • Assurance that site is compliant with NEC, IEEE and TIA/EIA standards
Important Points:
PowerAudit® Yearly Review is available in North America only.