APC will perform a once a year visual and electronic inspection of the UPS system to ensure that the system is performing to all technical and environmental specifications. In addition to these inspections, APC will ensure that the UPS system is operating within all safety parameters.
This service includes:
- UPS environment is within specified operating conditions
- Verify proper airflow of fans
- Check UPS event log of any alarms and record log
- Check all power terminals of UPS under load
- Check all remaining terminations not previously checked
- Spot-check terminal temperature of internal or external batteries
- Verify actual voltage and current to the UPS display
- Perform discharge test
- Verify proper transfer to battery operation
- Test internal static bypass
- Clean all dust and debris from UPS
- Inspect the capacitor banks for damage (if applicable)
- Check inside the UPS that all control wires and power wires are properly seated and undamaged
- Physically torque all power connections inside UPS system
|
 |
Benefits to Customer:
- Maximize uptime through preventative maintenance
- Includes proactive parts replacement in years 3 to 5
- Optimize lifetime of the product
- Security against unplanned outage of critical systems
- Full status of all on-site activities delivered to customer
Important Points:
- This service is provided as part of the Premium and Enterprise Power Reliability packages as well as the Annual Maintenance Program.
- If additional Preventative Maintenance Visits (PMV) are required in one years time, then this service may be ordered as an upgrade to the Power Reliability Packages as well as the Annual Maintenance Program. Order on PMV for each additional visit required in the one year contract.
- Allow for a two week lead time in service scheduling
- Part Number to order as upgrade to service package: WPMV-T
|
|