APC will provide guidance as to how to physically connect the 3-Phase UPS to the mains. The actual electrical connection will be accomplished by a customer designated electrician or an APC referred electrical contractor. In either case, APC Authorized Personnel will be on-site to oversee the installation of the product.

APC will:
  • Meet with customer to understand UPS environment requirements
  • Evaluate accessibility for delivery of UPS:
    Sizing requirement for entryways/hallways
    Suitable delivery path
    Acceptable floor loading (rolling)
  • Evaluate suitability of UPS environment:
    Air conditioning consumption
    Pacing requirements
    UPS electrical configuration
    Acceptable floor loading (rolling)
  • Meet with installing electrician to review electrical installation requirements


Benefits to Customer:
  • Customer resources freed to concentrate on core business focuses
  • Assurance of proper installation
  • Ease of installation
Important Points:
  • Customer designated electrician or an APC referred electrical contractor will accomplish the actual electrical connections
  • Customer supplies electrical equipment up to the connection point of the UPS
  • Customer may choose in-house electricians, their own contractor or and APC designated contractor
  • Allow for a two week lead time in scheduling
  • APC is not responsible for wiring before and after UPS
  • APC will be present during the installation
  • Service is part of Premium and Enterprise Power Reliability programs
  • Part Number: WICS