Technical FAQs

Ask a Question

Galaxy VM: Comparison of the following Configuration / modes of operations

 
 
Issue:
Galaxy VM: Comparison of the following Configuration / modes of operations
 
  1. Normal Mode Operation
  2. ECO Mode Operation
  3. ECOnversion Operation
 
Product line:
All Galaxy VM 3 phase Products
 

Environment:
All models, All serial numbers
 

Cause:
Inform about the comparison between the operation modes
 

Resolution:
We publish this information to clarify the operation modes and the electrical parameters of the different operation modes for Galaxy VM products
 

 
 
 
 

 
Was this helpful?
What can we do to improve the information ?