Pelco camera presets configured on the NetBotz appliance are saved on the camera using a default naming convention
Issue:
Pelco camera presets configured on the NetBotz appliance are saved on the camera using a default naming convention rather than the preset names configured in the NetBotz appliance user interface.
Product Line:
NetBotz, Pelco
Environment:
NetBotz, Pelco
Cause:
This is a known limitation of the integration between the NetBotz appliance and Pelco cameras.