StruxureWare Central, StruxureWare Data Center Expert.
Environment:
Upgrade from version 7 to version 7.2.
Cause:
Missing configuration.
Resolution:
Upon upgrading from StruxureWare Central version 7.0 to StruxureWare Data Center Expert version 7.2, any non default HTTPS port will not be retained. The HTTPS port will be reset to 443. The only resolution is to log in to the system and manually reconfigure the port. 7.2.1 resolved this issue so instead of upgrading from 7.0 to 7.2 (which is no longer available) the current 7.2.1 upgrade does not see this issue.