Expired Certificate Warning When Installing NetBotz Central Console
Issue:
Expired Certificate Warning When Installing NetBotz Central Console
Product Line:
NetBotz Central
Environment:
NetBotz Central (any version)
Cause:
Expired Certificate Warning
Resolution:
On systems that have older version JRE`s when installing the The NetBotz Central console from the NetBotz Central server web page there can be a prompt that the certificate has expired. The certificate is actually not expired and the install can be completed by selecting Yes to continue.