Power Protection Strategy

Choose between centralized, zone, or distributed power availability architecture

Centralized power availability architecture

SilconThe "Centralized" power availability solution is the traditional approach to selecting power availability for a large project. Estimate the total load expected over the life of the project. Select a UPS with enough headroom to accomodate the estimate. APC's Silcon family offers a power factor corrected design with the ability to build in N+1 redundancy to your network power infrastructure. Silcon's small footprint makes an excellent choice for large centralized power requirements.

Symmetra Zone power availability architecture
The "Zone-based" power availability solution for a fast growing business breaks down the total load into more manageable segments. Able to power multiple racks of network equipment, APC's scalable Symmetra Power Array protects a "zone." The modular design of this UPS allows the user to configure a single chassis from 4kVA up to a fully loaded 16kVA. The system power grows with the business. As the "zone" of equipment taps the capacity of the UPS another zone may be started on another Symmetra chassis. This "zone-based" architecture uses precious corporate capital more efficiently and raises the ROI of the investment in power availability.

PowerStackDistributed power availability architecture
The "Distributed" power availability solution uses smaller individual APC Smart-UPS to protect a single rack of equipment. As the number of racks grows within the business, the number of UPSs grows in direct proportion. This power architecture solution could be used where there are tight capital constraints on a business which prohibit a large outlay of funding for unused power infrastructure.

APC Global Services (AGS)
APC's Global Services Group provides comprehensive end-to-end service and support to APC customers and partners around the world. Our goal is to provide a continuous supply of power to our customer's systems, networks, and facilities, regardless of circumstances.