ASK THE EXPERTS

Q:What is the expected life of an APC UPS battery? 

A: All APC batteries should last three to five years. Below are some guidelines to ensure optimum life expectancy:

1. Make sure that the APC UPS battery is kept in a cool, dry location with plenty of ventilation. Ideally, the temperature where a UPS is kept should not exceed 75° F (24° C). Also, for ventilation purposes, leave roughly one to two inches on each side for proper airflow.

2. Only perform runtime calibrations on the UPS one or two times a year, if necessary. Some of our customers want to check their systems to verify that their runtime is sufficient. However, consistently performing these calibrations can significantly decrease the life expectancy of your APC battery. Click here for more information on runtime calibration.

3. Do not store APC batteries for extended periods of time. New batteries can be stored for 6 to 12 months. After this period, the battery should be used or it will lose a great deal of its charge. It is not advisable to store batteries that have already been in use.

4. Do not exceed 80 percent of a UPS unit’s rated capacity due to the reduction in run time. When loads increase, runtime lessens. In the event of a power failure, a UPS loaded to full capacity will drain and discharge its battery quickly and will lessen the life expectancy.

Purchase options for your UPS battery:

How to purchase replacement UPS batteries

UPS Upgrade Selector

Other free resources and documentation from APC you may be interested in:

White Paper #15 helps explain the differences between Watts and VA and how the terms are often incorrectly used to specify power protection equipment.

White Paper #18 will explain the most common types of power disturbances, what can cause them, what they can do to your critical equipment, and how to safeguard your equipment.

White Paper #30 looks at why lead-acid batteries are the predominant choice for UPS energy storage. This paper discusses the advantages and disadvantages of this and two other types of UPS batteries. 



01/12/2007
 
Send this APC solution to a friend or colleague

APC will not store the email address that you are providing to us and therefore will not use it for marketing communications. Only those customers that have indicated will receive email marketing communications from APC.

Back