Technical FAQs

Ask a Question

How to reset an Air Filter Run Hours violation alarm on a Uniflair Unit

Issue:
How to reset an Air Filter Run Hours violation alarm on a Uniflair Unit
 
Product line:
All Unfair Units with Push-Button Display, All Chilled Water Uniflairs.
 
Environment:
All Serial Number with Push-Button Units
 
Cause:
Repair, Install, Maintenance
 
Resolution
 
To clear Air filters run  hour violations from a Uniflair push button display.
 
Press <> PRG
 
Settings Menu <> ENTER
 
Code <> 00000 ENTER
 
Hour-Meter Settings <> ENTER
 
ENTER down to reset hit ENTER change display to OK and then ENTER Again.
 
Alarm has been cleared
 
 
Was this helpful?
What can we do to improve the information ?