Technical FAQs

Ask a Question

Data Center Operation | How do I reset the client password?

Issue:
How do I reset the password for the StruxureWare Data Center Operation client?

Product Line:
StruxureWare Data Center Operation (DCO)

Environment: 
StruxureWare Data Center Operation 8.x (DCO)

Cause: 
Password for logging into the Data Center Operation client has been lost or forgotten.

Resolution:

To regain access to the web or desktop client of Data Center Operation, you can have another user with administrative credentials reset your password. This can be done via the web interface of Data Center Operation under Administration -> Users -> "Click on the User" -> Reset Password.

If no other user has an administrator account or you are the only user, please contact your local technical support for assistance.

To contact local support, please see the following link for contact information:
www.apc.com/support/contact/index.cfm
Was this helpful?
What can we do to improve the information ?