Technical FAQs

Ask a Question

What are the hole sizes and dimensions of the AR8395 copper bus bar?

Issue:
A customer wants to use 2-hole lugs on the ground bar

Product Line:
NetShelter Bus Bar

Environment: 
AR8395

Cause:
Grounding / bonding is required

Resolution: 
The AR8395 has the following holes available: 
47 holes threaded #10-32, spaced 18 cm center to center. 
25 holes at 5.5 cm and 9 holes at 7.9 cm, spaced at 25 cm center to center. 
 
Was this helpful?
What can we do to improve the information ?