Technical FAQs

Ask a Question

Video: How to change Service Intervals of an InRow ACRD200 cooling unit

Issue:
How to change Service Intervals of an InRow ACRD200 cooling unit

Product line:
InRow ACRD200

Environment:
All Serial Numbers

Cause:
Install, Configuration

Resolution:



Press ESC until you get to the main screen (On/Standby)
 
Use the Up or Down arrows to find the heading Service Intervals
 
Press ENTER
 
Now you will be prompted for a password
 
Use the default password of “apc”
 
If this does not work check with your Admin for the correct password
 
If password has been lost use the last eight digits of the serial number
 
Press Enter on Interval and select the number of weeks you would like the alarm to return
 
Press Enter on Alarm and select to enable or disable the alarm
 
Was this helpful?
What can we do to improve the information ?