Technical FAQs

Ask a Question

DG5 Modbus Register Map

Issue:
DG5 Modbus Register Map   

Product line:
Airflow with DG5 Board  

Environment:
Airflow with DG5 Board 

Cause:  

Resolution:
See Attached Document

Default Modbus Serial Settings
Baud 9600
Bits 8
Parity None
Stop Bits 1
Flow Control None

Was this helpful?
What can we do to improve the information ?