Technical FAQs

Ask a Question

How should the AR7701 be oriented for installation?

Proper orientation for the AR7701 is requested. It appears that the AR7701 can be installed two different ways.

Product Line:
NetShelter SX

All versions and serial ranges.

To install the AR7701 on a cabinet with no castors it must be installed upside down.

The AR7701 is intended to be a universal bracket that can be installed in either orientation depending on which fits the installation best. One orientation requires removal of the castors.
For illustration please see the attached file.

Was this helpful?
What can we do to improve the information ?