Technical FAQs

Ask a Question

Trial version of StruxureWare Data Center Expert VM appears to have 25 nodes available.

Issue:
Trial version of StruxureWare Data Center Expert appears to have 25 node license available.

Product Line:
StruxureWare Data Center Expert

Environment:
AP94VMTRL  any version.

Cause:
The current default configuration of all StruxureWare Data Center Expert is that the system comes with a pre-installed 25 node license key. The Virtual Machine or VM version shows this same 25 node license key in the user interface however until activated, will only allow 5 nodes to be added to the system.

Resolution:
This is by design. It was done so APC did not need to add a 5 node key to just this one version.  Once activated, the rest of the nodes can be used.
 
Was this helpful?
What can we do to improve the information ?