Can the NetShelter CX be deployed in any room or space?
Issue:
Where can the NetShelter CX be deployed?
Product Line:
NetShelter CX
Environment:
All versions and serial ranges.
Cause:
Customers want to make sure that the NetShelter CX is suited for the environment in which they intend to install it.
Resolution:
Optimal performance of these cabinets requires suitably ventilated space or building HVAC system.
The NetShelter CX is not suitable for installation in a small unventilated space.